Cancel
Showing results for 
Search instead for 
Did you mean: 

JTTK 8.0, Can't import SOME .JT files

Experimenter
Experimenter

Good day.

 

With the JTTK 8.0, it is not possible to import some specific JT files (can't open). This problem only occurs for JT files that are processed by a tool from one of our costumers.

 

JT Utilities (like jtattribute.exe) also cannot open this specific files. For the record, older versions of JT Utilities CAN open this same files, however, with the latest JT Utilities 10.0 this is not possible.

 

This jt files can be opened by teamcenter or any other JT viewer.

 

 

Any hint on this problem?

Thanks in advance

3 REPLIES

Re: JTTK 8.0, Can't import SOME .JT files

Valued Contributor
Valued Contributor
Is this a standalone .jt file or is it split in sub JT files ?

Re: JTTK 8.0, Can't import SOME .JT files

Experimenter
Experimenter

This are monolithic JTs, so single .JTs

 

This kind of JTs have been processed by a tool, that add some attributes to the file. The file can be opened normally with Teamcenter, NX, or older versions of JT Toolkit /JT Utilities. However with the latest JT Toolkit  (8.0) or the JT Utilities 10.0 (which I assume use the same libary versions) the import always fails.

 

Is there any way to check what makes this JTs different? or why the latest version of JtTk fails to import them?

 

Thanks and greetings

Re: JTTK 8.0, Can't import SOME .JT files

Valued Contributor
Valued Contributor

Hi PedroS,

Did you find any hint on this issue ?

 

Nicolas