Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with JT open Toolkit

Experimenter
Experimenter

Hi Experts!

Recently, i have  downloaded the JT open Toolkit. I installed it according to the Siemens Guidance and then Firstly i tried to follow the Get_Started_Doc in the Program and wanted to open the Geom_Simple Example. After i did so and also gave my Sold_To_ID, i tried to run the app, but i got some weird Errors as below :

 

'geometry_VS2013_Win32_Debug.exe' (Win32): Loaded 'C:\Program Files (x86)\Siemens\JTOpenToolkit\8_5\example\Geom_simple\geometry_VS2013_Win32_Debug.exe'. Symbols loaded.
'geometry_VS2013_Win32_Debug.exe' (Win32): Loaded 'C:\Windows\SysWOW64\ntdll.dll'. Cannot find or open the PDB file.
'geometry_VS2013_Win32_Debug.exe' (Win32): Loaded 'C:\Windows\SysWOW64\kernel32.dll'. Cannot find or open the PDB file.
'geometry_VS2013_Win32_Debug.exe' (Win32): Unloaded 'C:\Windows\SysWOW64\kernel32.dll'
'geometry_VS2013_Win32_Debug.exe' (Win32): Loaded 'C:\Windows\SysWOW64\kernel32.dll'. Cannot find or open the PDB file.
'geometry_VS2013_Win32_Debug.exe' (Win32): Loaded 'C:\Windows\SysWOW64\KernelBase.dll'. Cannot find or open the PDB file.
'geometry_VS2013_Win32_Debug.exe' (Win32): Loaded 'C:\Windows\SysWOW64\apphelp.dll'. Cannot find or open the PDB file.
'geometry_VS2013_Win32_Debug.exe' (Win32): Loaded 'C:\Windows\SysWOW64\msvcp140d.dll'. Cannot find or open the PDB file.
'geometry_VS2013_Win32_Debug.exe' (Win32): Loaded 'C:\Windows\SysWOW64\vcruntime140d.dll'. Cannot find or open the PDB file.
'geometry_VS2013_Win32_Debug.exe' (Win32): Loaded 'C:\Windows\SysWOW64\ucrtbased.dll'. Cannot find or open the PDB file.
The thread 0xa14 has exited with code -1073741701 (0xc000007b).
The thread 0x4ed4 has exited with code -1073741701 (0xc000007b).
The thread 0x47f8 has exited with code -1073741701 (0xc000007b).
The program '[20356] geometry_VS2013_Win32_Debug.exe' has exited with code -1073741701 (0xc000007b).
 
I have already read the software prerequisite (e.g. Visual Studio 2015) and install them too, what would be the Problem and how can i solve it?
 
my final intention is to open .JT file and just see that and may transform it.
 
I would be grateful of any help and answer.
 
1 REPLY

Re: Problem with JT open Toolkit

Genius
Genius

Try these steps and let me know if it resolves your issue

 

Make sure your environment variables are set up properly

JTTK_DEV_PATH=C:\Program Files (x86)\Siemens\JTOpenToolkit\8_5\dev
JTTK_DEV_PLATFORM= 64_VS2013
JTUTILITIES_PLATFORM= 64_VS2013

 

1. First open the "License" project file (license_check_VS2013.vcxproj) In the "License" example, uncomment the following line. Note: Use your sold-to ID (not your JT toolkit license key) and take off the zeros at the beginning! So if your sold-to ID is 0001234567, take off those 3 zeros at the beginning like so.

 

JtkEntityFactory::registerCustomer(1234567);

 

2. Right-click on the project file and clicked "Build". Note: You may have to grant administrator rights to your JTOpen folder for some reason. In Windows Explorer, you can just do this by right clicking on the JTOpen toolkit directory and granting read/write privileges.

 

3. Open up the project file for your example. For the "Geometry Simple" example, it would be "geometry_VS2013.vcxproj"

 

4. In "main.cpp" for your example, uncomment the following line

JtkEntityFactory::registerCustomer(1234567);

5. Build your solution. Note: Click on properties in Visual Studio and make sure you are configured for the x64 platform 

  

6. If there are no errors in your code, then an executable (.exe) should now be there. 

7. Run the .exe and your JT file should be generated!