Cancel
Showing results for 
Search instead for 
Did you mean: 

Why is import in JTOpenToolkit so slow compared to JT2Go ???

Experimenter
Experimenter

Hi Folks,

 

I noticed a considerable latency when loading a JT model with JT OpenToolkit.

 

I tried any import option combination possible, even exluding everything (Geometries, Brep, PMI,...)

 

The model that I use is fairly large (5000 hierarchy nodes) but in comparaison the JT2Go viewer is able to load absolutely everything very fast.

 

With JT2Go in less than a few seconds the full model is loaded and displayed, whereas it sometimes takes me a whole minute until the same model is simply imported in JTOpenTK.

 

Does that mean that JT2Go uses a home brewed JT loader and that JTOpenToolkit is not as optimized at it could be ?

 

Please help me figuring this one out.

2 REPLIES

Re: Why is import in JTOpenToolkit so slow compared to JT2Go ???

Siemens Genius Siemens Genius
Siemens Genius

Hi,

This is a common observation, JT2Go is using the same technology to load JT files but makes use of late loading features not currently supported in the Toolkit. The toolkit loads the entire file  before returning. We did add a new feature in the 8.5 release of JTTK where by users can make call backs as the file is loading. This doesn't really make the file load faster but does allow for response while the file is loading.

We are now looking at adding a late loading capability to JTTK in the next release, Q1 2018

Mike Z

Mike Z

Re: Why is import in JTOpenToolkit so slow compared to JT2Go ???

Experimenter
Experimenter

Neat, thanks for your enlighting answer.

What is JT?

JT is the World’s Most Widely Used 3D File Format for PLM

JT is the common language of PLM and is the world’s most widely used 3D format. JT is the first ISO International Standard ( IS 14306-1) for 3D visualization and collaboration. Compact and accurate, JT is used throughout the product development lifecycle in all major industries to communicate the critical design information typically locked up inside a CAD file.

Siemens PLM Software customers rely on JT to be the most robust 3D visualization format available.

JT Open Factsheet
JT Open Member Resources
JT Open Documentation Technology
JT Open File Format Technology
JT Open Toolkit

Downloadable viewers for Windows Desktop, Windows 10 Universal App, Android and iOS.


Download JT2Go for your platform today Download JT2Go Desktop 64 Bit all languages
Download JT2Go Desktop 32 Bit for English
Windows 10 JT2Go Universal App
Android JT2Go
iOS JT2Go