Cancel
Showing results for 
Search instead for 
Did you mean: 

Create PDF with JT command

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Discovering JT2GO V11.2.0, there is a promising "Create PDF with JT" in the Menu / JT2GO.

Why in my session this capability is Grey Out ?

 

I have setup my acrobat reader V11 as desvribe in the doc.

 

May i install something else ?

 

Regards

2 REPLIES

Re: Create PDF with JT command

Siemens Genius Siemens Genius
Siemens Genius

The create .pdf option is greyed out when there are no model views selected. Depending on your setting for model view load options (default is by node) there may not be model views available to produce .pdf output from at the node you have selected in the product structure tree.

One option is to turn on the Model View Snapshots, as you navigate the tree the snapshots will update with the model views available . The create pdf option will output the model views visible in the snapshot gallery.

Mike Z

Re: Create PDF with JT command

Pioneer
Pioneer

Mike,

 

I have JT2GO 11.4.0 and I don't see Create PDF with JT at all in the JT2GO->Attachments menu.

 

I have Model Views, thumbnails etc. Why am I not seeing the "Create PDF with JT" button?

 

Thanks,
Sameer

What is JT?

JT is the World’s Most Widely Used 3D File Format for PLM

JT is the common language of PLM and is the world’s most widely used 3D format. JT is the first ISO International Standard ( IS 14306-1) for 3D visualization and collaboration. Compact and accurate, JT is used throughout the product development lifecycle in all major industries to communicate the critical design information typically locked up inside a CAD file.

Siemens PLM Software customers rely on JT to be the most robust 3D visualization format available.

JT Open Factsheet
JT Open Member Resources
JT Open Documentation Technology
JT Open File Format Technology
JT Open Toolkit

Downloadable viewers for Windows Desktop, Windows 10 Universal App, Android and iOS.


Download JT2Go for your platform today Download JT2Go Desktop 64 Bit all languages
Download JT2Go Desktop 32 Bit for English
Windows 10 JT2Go Universal App
Android JT2Go
iOS JT2Go