Cancel
Showing results for 
Search instead for 
Did you mean: 

JT2GO & MS Word integration

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi,

I use Win7 x64. I installed JT2GO v.10.1.4 and after that installed MS Office x86. If i try to open example (Start->Teamcenter 10.1->Lifecycle Visualization->JT Documents Examples->MS Word JT Document), then I get error message in MS Word (see image below). How it could be fixed?

img01.png

7 REPLIES

Re: JT2GO & MS Word integration

Siemens Legend Siemens Legend
Siemens Legend

Try using PLMVisOCX1.SetFile instead of PLMVisOCX1.File.

Re: JT2GO & MS Word integration

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Did not help Smiley Sad

Re: JT2GO & MS Word integration

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

I found out that 2 modules is missing. It is WebTree.ocx and PLMVisOCX.ocx

img02.png

Re: JT2GO & MS Word integration

Siemens Legend Siemens Legend
Siemens Legend

Hi,

 

I was able to reproduce what you are seeing.  After talking with the development team, the problem is the example file was never updated when the PLMVisOCX and WebTree were deprecated out of the product and replaced with the VisJt2GoOCX.

 

Rick

Re: JT2GO & MS Word integration

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi Riky,
If it is problem with example file, it's ok.
But, when I try add jt file into MS Word Document I get message (see message below, sorry, message in russian, but I translated it bellow)

 

img03.png

 

I use in MS Word:
Insert -> Object -> Create from file

 

After that I choose jt file (see file model.jt in attach) and get message with meaning:
Object was created in the program: DirectModel. This program not installed on your computer or not response. For modify the object, install DirectModel or make sure that all dialog windows are closed.

 

JT2GO installed and not open at the moment.

 

img04.png

 

What is wrong?

Re: JT2GO & MS Word integration

Siemens Legend Siemens Legend
Siemens Legend

This was a known issue with unsupported languages which has been resolved.   See this post on the forum for the solution:  http://community.plm.automation.siemens.com/t5/JT2Go-Forum/Solution-to-the-problem-quot-The-program-...

 

It specifies JT2Go 10.1.5, but it should work for 10.1.4 - if it doesn't, please update to 10.1.5 (Download JT2Go Desktop 32 bit version for English on the JT2Go home page - https://www.plm.automation.siemens.com/en_us/products/teamcenter/plm-platform-capabilities/visualiza...).

 

Re: JT2GO & MS Word integration

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

RickY, thank you very much! It is work properly now!

Smiley Happy