Cancel
Showing results for 
Search instead for 
Did you mean: 

JT2GO does has any command line utility to open given JT file and Attach 2D PDF file automatically

Experimenter
Experimenter

Hello,

 

I searched in JT2GO OOTB dump installed and verfied in help. I could not find any information on to do some automation using cmd line utility to handle the requirement as follows.

Open the given JT file form disk or database and attache file of 2D PDF file either from disk or from database.

I would like to check if JT2GO do not have this capability do JTOpen Toolkit can able to achieve these kind of automation requirements?

 

regards,

kishore

3 REPLIES

Re: JT2GO does has any command line utility to open given JT file and Attach 2D PDF file automatical

Experimenter
Experimenter

I could able to solve thise issue, we have the utility in OOTB under the JT2GO installation.Here you go JT2Go\Program\2DPDF\PDFJTExtractor.exe

Note: It can do both export and attach.

Re: JT2GO does has any command line utility to open given JT file and Attach 2D PDF file automatical

Pioneer
Pioneer

I just installed JT2GO 11.4 and I don't see this folder ( C:\Program Files\Siemens\JT2Go\Program\2DPDF ) in th OOTB installation.

 

Where else can I get PDFJTExtractor.exe from?

Re: JT2GO does has any command line utility to open given JT file and Attach 2D PDF file automatical

Experimenter
Experimenter

Hi,

 

You suppose to get the exe in the same location, i am not sure why it is not exist in the folder as you mentioned.

I am using lower version than your's it exist in the same location. Let try to re-install and check or search the exe in the top level folder,chace of moving this utility to any other sub directory under JT2Go.

 

regards,

kishore