Cancel
Showing results for 
Search instead for 
Did you mean: 

JT2Go 11.3 and JT2Go 11.3 Desktop App differences

Gears Legend Gears Legend
Gears Legend

Hello,

have seen it is also new existing a JT2Go 11.3 Desktop Windows 10 app.

Before JT2Go 11.3 for Windows can open Solid Edge files it is written for JT2Go 11.3 Desktop Windows 10 app that it can open Solid Edge files.

Have done a test with JT2Go 11.3 Desktop Windows 10 app and it cannot open Solid Edge files.

Therefore, I check the JT2Go Desktop app version and find out it is different to JT2Go Desktop version.

Now to the question can JT2Go Desktop app already open Solid Edge files or need it an update in the Windows App Store?

Best RegardsPLMXML_error_JT2Go_113_Desktop_app_open_SE_file.PNG

Wolfgang

 

 

3 REPLIES

Re: JT2Go 11.3 and JT2Go 11.3 Desktop App differences

Siemens Legend Siemens Legend
Siemens Legend

Yes, they are slightly different (Windows 10 App is 11.3, Windows 10 desktop is 11.3.0.1 a01), but both do support loading Solid Edge files, although there are some issues with some files.  JT2Go 11.4 will include updated Solid Edge file support, which should resolve loading problems.  11.4 is due to be released mid December 2017.

Re: JT2Go 11.3 and JT2Go 11.3 Desktop App differences

Gears Legend Gears Legend
Gears Legend
Thank you, hope it will work for both versions.

Re: JT2Go 11.3 and JT2Go 11.3 Desktop App differences

Siemens Legend Siemens Legend
Siemens Legend

You will still see some issues in viewing, depending on the version of your solid edge files.  We have found that newer files do show some color and PMI issues.  We have logged an ER against TcVis to get these issues resolved, as changes in the plmxml from SE are going to require changes in TcVis in order to properly handle the files.  What you have seen with being unable to open the plmxml may be another artifact of that upgrade.