Cancel
Showing results for 
Search instead for 
Did you mean: 

JY2go 3 points section

Creator
Creator

Is there anybody who know if on JT2go is possible to perform a section through 3 poins plane?

It seems to be possible create section only thourgh X,Y,Z axis..

 

Toni

 

5 REPLIES

Re: JY2go 3 points section

Gears Legend Gears Legend
Gears Legend

Hello Toni,

 

with JT2Go not possible.

It is Possible with TCvis or you use from Solid Edge a PMI section.

For PMI you must save the JT-File with PMI.

You find this in the option at saving under Solid Edge.

 

Wolfgang

Re: JY2go 3 points section

Creator
Creator

OK Thanks

Do you know guys here how to request an enhancement on JT2go? I know that there is a specific channel different from others SPLM sofware

 

Thanks

 

Re: JY2go 3 points section

Gears Legend Gears Legend
Gears Legend

Hi Toni,

 

if you ask for additional freeware for desktops based on PLMvis there are

 

freeware

Xpresreview 10.1.3 (32 bit based on PLMvis 10)

Solid Edge (free) Viewer 9 (32 bit based on PLMvis 10)

JT2Go 10.1.5 (32 bit based on PLMvis 10)

JT2Go 11.2.2 (based on PLMvis 11)

 

non Freeware

Inside Connect EN / View and Markup DE (32 bit based on PLMvis 10)

Teamcenter Life.. Visualisation (32/64 bit based on PLMvis 11)

NX Cam Viewer (64[32?] bit in parts based on PLMvis 11)

 

for use with additional funktions I think Teamcenter Life... Vis is the best version.

https://www.plm.automation.siemens.com/de_de/products/teamcenter/plm-platform-capabilities/visualiza...

 

for working with freeware with differend funktion I think you need a combination from

Xpresreview 10.1.3

Solid Edge (free) Viewer 9

JT2Go 10.1.5

this ones has the same base.

 

hope this helps

 

Wolfgang

 

 

 

Re: JY2go 3 points section

Creator
Creator

HI Wolfgang,

No, I was just asking how to request one more features on JT2g0.

How can I request in general enhancements to the sofware?

 

Toni

 

Re: JY2go 3 points section

Siemens Legend Siemens Legend
Siemens Legend

Hi Toni,

 

To request an enhancement to JT2Go, you have to be a JT Open program member and can request them through the Siemens GTAC website.

 

As for the 3-point cross section, that is a paid for feature of Teamcenter Visualization and cannot be added to JT2Go, as it is a free product.

 

Rick