Cancel
Showing results for 
Search instead for 
Did you mean: 

Missing functionality

Master
Master
Hi all,

First of all: Thank you for this great app Siemens PLM, we love it!


We are missing the following functionality:

- Part Attributes, to identifie parts numbers and our information stored in parts.
- Search for componnets whit specific part attributes
- Simple Measures, to get a "missing" dimension on the 2D Drawing quickly.
- Section View, to see inside the part.
- Set the selected component as "Work" and other as translucent.


Are there any plans to include one of this functionality in the future?
5 REPLIES

Re: Missing functionality

Experimenter
Experimenter
Thanks for your comments, we are considering improvements to the viewer so stay tuned.

Re: Missing functionality

Siemens Pioneer Siemens Pioneer
Siemens Pioneer
You can access part attributes by selecting/highlighting a single part only. Once only a single part is selected/highlighted, the "Model Properties" menu option is replaced with "Part Properties". Selecting this menu option will show properties for the selected part. If nothing is selected, or multiple parts are selected, then the "Model Properties" menu option is shown.
Steve Menyhart

Re: Missing functionality

Master
Master
I can see this area. It not shows me our user attributes
We have about 60 part attributes.
Maybe because we create the JT file from NX8?
I have set the "getAttributes = true".


Re: Missing functionality

Siemens Pioneer Siemens Pioneer
Siemens Pioneer
Could you please try using the Assembly tree view to select a node one level up from the part you wish to view properties for? For example, in the picture you posted, instead of selecting "9736-sr-el1-ta_76", select its parent "9736-sr-el1-ta". Then see if your missing user properties are on that node.

If this doesn't work, please load this same JT file on the Windows Desktop version of JT2Go and see if you can see the missing properties.
Steve Menyhart

Re: Missing functionality

Master
Master
I know that "9736-sr-el1-ta_76" its the solid body and "9736-sr-el1-ta" its the component.
The attributes are part attributes so they should be on the component.
But the are not there