Cancel
Showing results for 
Search instead for 
Did you mean: 

Open step files

Valued Contributor
Valued Contributor

As a NX/TC user I work with JT files, but I cant use them to tranfer geometry to suppliers/clients because most of them cant open JT files. So they ask me to convert the geometry to step, iges... Most people doest know about JT2GO because it is not useful for them. In my oppinion if JT2GO were able to be used as free visor not only for JT files but also for step, iges... more people would have JT2GO installed so JT files would be more used too. Maybe even if it were able to convert JT to step even better for make JT a more used format.

4 REPLIES

Re: Open step files

Siemens Legend Siemens Legend
Siemens Legend

Since a version of JT2Go is not specificied in your post, I will presume you are talking about the desktop version of JT2Go on Windows.  If you can export your files to STEP 242, JT2Go 11.2.3 is able to load those types of files.  Other conversions from Step to JT and IGES to JT are not supported, because they are paid for features of Teamcenter Visualization, which JT2Go desktop is based on, and cannot be given away for free.

 

Rick

Re: Open step files

Siemens Phenom Siemens Phenom
Siemens Phenom

@RickV If I am not wrong to export STEP242 from NX, it requires additional/special license.

 

Re: Open step files

Siemens Legend Siemens Legend
Siemens Legend

Then I afraid I cannot help further.  JT2Go is not able to load STEP or IGES files.

 

Rick

Re: Open step files

Valued Contributor
Valued Contributor

I just wanted to say to Siemens PLM people what I think would help to spread use of JT files on the industry. Maybe I am wrong, but I think is good to share oppinion. Thank you Rick anyway.