Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

PMI's are not displayed in JT2Go 12.2

Experimenter
Experimenter

Used Versions:

  • Creo Version: 5.0.2.0
  • JT-Translator Version: 14.1
  • JT2Go Version: 12.2

 

There have been two problems which occurred to me when using JT2Go version 12.2:

 

1.

If this JT assembly is opened in JT2Go version 12.2, only one combined-view is shown. If the same JT assembly is opened in JT2Go version 11.4, eleven different combined-views are shown.

So in version 12.2 some combined-views are not being loaded/shown, even though this is the case in JT2Go version 11.4.

 

2.

If a combined-view is selected in JT2Go version 12.2, a bunch of PMI's are not being loaded/shown. If the same combined-view is selected in JT2Go version 11.4, the combined-view with it's PMI's are displayed correctly.

 

 

So in both cases it has something to do with version 12.2, since it used to be working in version 11.4.

This happened to other JT assemblies as well, I am just using this one as an example.

I attached a screenshot of each version where both of the described problems can be seen.

2 REPLIES 2

Re: PMI's are not displayed in JT2Go 12.2

Siemens Phenom Siemens Phenom
Siemens Phenom

If you have Teamcenter Visualization, can you reproduce the issue there?

 

Any chance you can attach one of the jt files/assemblies that shows the issue to this post?

 

Thanks,

Rick

 

 

Re: PMI's are not displayed in JT2Go 12.2

Experimenter
Experimenter

Unfortunately I cannot atatach the jt files I've used.

 

I have tried it with Teamcenter Visualization Mockup 12.2.

The combined views are all shown correctly, but the PMI's are still missing.

 

 

I opened a SPLM GTAC Ticket for this case.

 

Thank you for your help.

Jon