Cancel
Showing results for 
Search instead for 
Did you mean: 

Perspective of part

Experimenter
Experimenter
Hello, I have an second problem with one workstation. When I open the jt-Part the view have an perspective (see the attachment "Teile_ansicht_1.jpg") . When I open the part on an other workstation the part looks well (Attachment "Teile_ansicht_2.jpg"). Second Problem on the first Workstation: The menu "JT2GO" is shown greyed (Attachmend "Menue_JT2GO_1.jpg"). I have controlles the software settings from the both workstations. In the Hardware we have a diffrent in the graphic (Intel HD vs nvidia Quadro) Have anyone an ideal. Best regards knwww
3 REPLIES

Re: Perspective of part

Valued Contributor
Valued Contributor

Hello,

yes it is an different between the GPU.
you can change the open GL setting.

Es gibt einen Unterschied bei den GPU´s
Du kannst die Open GL Einstellungen ändern.

 

Under View/Ansicht (desk/main view mouse right klick / or buttonbar view) performants/Leistungseinstellungen then/dann

Fehlerbehebung (Schieber für Open GL) move it left / nach rechts bewegen bis ok.

Re: Perspective of part

Experimenter
Experimenter

Hello,

when I make the different setting in the open-gl option. I see the part.

 

The Second Problem with the menu "JT2GO" is shown greyed is still existing.

 

Best regards

 

knwww

Re: Perspective of part

Valued Contributor
Valued Contributor
Well,
can not find the setting to solve the problem.
Have test if you can open it under the folder Menü -> JT2Go ?
there are the buttonbars also.