Cancel
Showing results for 
Search instead for 
Did you mean: 

Representation of the Color bar of NX 11 Simcenter results in JT2Go

Experimenter
Experimenter

In JT2Go (11.2.3) is the representation of the color bar spectum not comparabal with in NX (11.0.011) .
Is this a bug or can I influence this in NX or in JT2Go?


How I can influence the Colorbar that the color spectrum display is exactly like in NX. (see pictures)

 

Display_NX11.0.0.11.pngDisplay NX 11.0.0.11

 

 

Display_JT2go_11.2.3.pngDisplay JT2Go 11.2.3

 

 

 

2 REPLIES

Re: Representation of the Color bar of NX 11 Simcenter results in JT2Go

Siemens Legend Siemens Legend
Siemens Legend

The color bar displayed in Jt2Go is the same one you will see in TcVis (as JT2Go is based on TcVis).  Any questions regarding the display/configuration of the colorbar would have to be directed to the Teamcenter Visualization group.

 

Rick

Re: Representation of the Color bar of NX 11 Simcenter results in JT2Go

Experimenter
Experimenter

@RickV thanks a lot for you comment