Cancel
Showing results for 
Search instead for 
Did you mean: 

Solution to the problem "The program used to create this object is package", JT2Go 10.1.5 (32-bit).

Siemens Legend Siemens Legend
Siemens Legend

We are glad to announce that we have been able to identify and fix the JT2Go 10.1.5 (32-bit) Office Integration issue that results in the error message indicating "The program used to create this object is package" when dragging/dropping a JT file into an Office document.  This issue was related to using the JT2Go English version in unsupported foreign locales.

 

The solution is extract the VisJT2GoOCX.ocx from the attached 7-zip file and overlay it into the Program directory (likely C:\Program Files (x86)\Siemens\JT2Go\Program - if you used the default install location) of your JT2Go 10.1.5 installation.