Cancel
Showing results for 
Search instead for 
Did you mean: 

Using solid edge translation services exe to create a jt file

Builder
Builder

Edgers hope I posted in correct location for my topic.  Anyway I decided to test a short script but cant get it to work on a simple training file in ST6.  Nothing happens accept when I execute bat file from C:\ drive it copies the SolidEdgeTranslationServices.exe with 0 K to the C:\ drive and nothing happens.....

 

My goal ideally is to have the translation services exe file to open the assembly file show all and save to jt file in output.  I'll see if Jasons SE code web site might help me with SE API but if more code savy people can help that would be great.

 

@echo off

REM Convert *.asm to *.jt outside Solid Edge using translationservices.exe


C:\Program Files\Solid Edge ST6\Program>SolidEdgeTranslationServices.exe -i="C:\Program Files\Solid Edge ST6\Training\carrier.asm" -o=C:\carriertest.jt -t=jt

ST9
WIN 7Pro 64bit
DELL T5810 3.7-4Ghz 32Gb ECC
3 REPLIES

Re: Using solid edge translation services exe to create a jt file

Siemens Legend Siemens Legend
Siemens Legend

This is not the correct location for this post.

 

Rick

Re: Using solid edge translation services exe to create a jt file

Valued Contributor
Valued Contributor

Try posting in the solid edge forum:

http://community.plm.automation.siemens.com/t5/Solid-Edge-Forum/bd-p/solid-edge-forum

 

Kind regards,

 

Thomas Musters, Virtual Reality development for Design & Engineering, ASML


Production: {NX9, VisMockup, Unity}

Development: {C#, Java, VB} Testing: {-none-}

Re: Using solid edge translation services exe to create a jt file

Builder
Builder

Sorry for posting in wrong location

ST9
WIN 7Pro 64bit
DELL T5810 3.7-4Ghz 32Gb ECC