Cancel
Showing results for 
Search instead for 
Did you mean: 

General Information regarding Process Simulate Human

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi all,

 

I have following queries regarding human ergonomic simulation in Process simulate :

 

1.) While creating an operation, for example "Walk Operation", on what basis the software commutes the  standard time, and displayes it on the gantt chart? Is it based of MTM-1 or some other standard?

 

2.) I am able to simulate a particular scenario with normal commands like "Auto Grasp","Get" etc. I wanted  to     know about TSB and in what scenarios it should be used as opposed to standard commands?

 

 

I would appreciate any inputs regarding above mentioned queries.

 

Many thanks in advance

 

 

2 REPLIES

Re: General Information regarding Process Simulate Human

Siemens Legend Siemens Legend
Siemens Legend

Hi Varun,

 

1) When creating a non TSB walk operation:

The distance is measured

The operation duration is calculated using this distance and the walk speed

The default walk speed is based on MTM1 – and the user can override it in the user options:

hum_opt.png

 

 

When working with a non TSB simulation in PS on eMS / PS Standalone you can also link the operation to MTM codes. Select the human compound operation and invoke: “Edit MTM Information….”:

edt_mtm.png

 

 

 

This will bring up a UI where you can select MTM codes from the MTM timecards.

 

When creating TSB tasks - the times are also based on MTM standards.

For a TSB simulation you can see a list of all the resulting time codes by invoking, “Create Timing Report”:

tim_rep.png

 

 

 

 

2)

For most general human simulations the recommendation is to use TSB.

TSB provides a more intuitive UI to create the simulations, better what if analysis capabilities etc.

In addition TSB has the focus, and most new features will be supported only on TSB.

 

Some features e.g. kinematic operations and human automatically follow moving device - are still supported only with the non TSB operations.

 

You can then author part of the simulation with TSB – wrap the TSB simulation in a compound operation. Author parts of the simulation with the old non TSB operations, wrap this in a compound operation.

Create link as required between the two compound operations.

 

Best regards,

Pelle

Re: General Information regarding Process Simulate Human

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi Pelle,

 

Thanks for the information

 

Regards,

Varun