Cancel
Showing results for 
Search instead for 
Did you mean: 

Human scaling

Experimenter
Experimenter

Hello

I'm learning JackScript for developing a module.

 

From JackScript Tutorial

 

2.4.2. Human scaling

The method Human.Scale provides access to 'simple scaling', which depends only on the human figure's gender, height and weight:

          >>> jill = CreateFemale("jill")
          >>> jill.Scale(6*u.ft, 170*u.lb, 'female')

 

 

When I entered "jill.Scale(6*u.ft, 170*u.lb, 'female')" in JackScript console, Jack stopped working.

So I wonder how to scale the human figure's gender, height and weight with JackScript.

 

4 REPLIES

Re: Human scaling

Siemens Genius Siemens Genius
Siemens Genius
The Scale functionality on the human has been superseded with newer functionality that allows selection of the desired anthropometric database to use. Please try the following updated commands: >>> myHum = scene. >>> myHumAS = myHum._human.initAnthroscale('CDN_LF_97') <= Any of the database name options from the scaling dialog can be used. >>> stature = 175.0 >>> weight = 71.0 >>> myHumAS.scaleHeightNweight(stature, weight) Note that the API expects stature in cm and weight in kg.
UlrichRaschke

Re: Human scaling

Experimenter
Experimenter
Thank you for your answer!
But these commands still made an error. It said...

File "<console>", line 1, in <module>
File "jsPeabody.py", line 1762, in __getattr__
AttributeError: initAnthroscale

Ps. I also removed "_" from >>> myHumAS = myHum._human.initAnthroscale('CDN_LF_97')
Is it correct?

Re: Human scaling

Siemens Genius Siemens Genius
Siemens Genius

 

It could be that it was difficult to follow the commands due to the reformatting of the post.

I've pasted them here again, hopefully more readable:

 

>>> myHum = scene.human
>>> myHumAS = myHum._human.initAnthroscale('CDN_LF_97')
>>> stature = 175.0
>>> weight = 71.0
>>> myHumAS.scaleHeightNweight(stature, weight)

 

The "_" in the second line is correct.

Please give the steps another try.

UlrichRaschke

Re: Human scaling

Experimenter
Experimenter
Now It's work.
Thank you very much UlrichRaschke Smiley Happy