Cancel
Showing results for 
Search instead for 
Did you mean: 

Kinect V2 with Jack 8.0.1

Experimenter
Experimenter

I'm trying to connect kinect V2 with Jack 8.0.1 trial version. I downloaded the microsoft SDK V2 plug in and when I run kinect modules on Jack, it shows the green icon but the Jack-kinect dialog doesn't appeare.

I think V2 is incompatible, can it be possible?

Someone can use Jack 8.0.1 with V2 Kinect?

Can you help me to configure kinect in Jack 8?

 

Thanks

 

Alessandro

2 REPLIES 2

Re: Kinect V2 with Jack 8.0.1

Siemens Genius Siemens Genius
Siemens Genius

Hello,

Currently, only the first generation Kinect sensor is compatible with Jack.  With this sensor, v1.5 (to v1.8) of the SDK is recommended.

 

Thanks!

Re: Kinect V2 with Jack 8.0.1

Experimenter
Experimenter
Hello,

Is Kinect V2 compatible with Jack now? Since I just got the new Kinect V2 and Adapter, but the Kinect-Jack interface didn't show up when I started it.

Thank you!