Cancel
Showing results for 
Search instead for 
Did you mean: 

Kinect for Jack

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi all,

 

Please help me out with the following queries,

 

1.) Are all the kinect devices(versions) compatible with all the versions of Jack and process simulate human. If not, is there a document which mentions the compatibility of Jack with the hardware?

 

2.) Can we simulate jack's interaction with various objects using kinect device, i.e., picking up an object or human holding a device like phone etc.?

 

Many thanks in advance,

 

-Varun

2 REPLIES 2
Highlighted

Re: Kinect for Jack

Siemens Genius Siemens Genius
Siemens Genius

Hi Varun -

 

Jack products (Jack and PS Human) are compatible only with the Kinect for Windows v1 sensor.

 

Object tracking is not supported with the Kinect as it uses the Kinect skeleton, which does not recognize objects.

 

 

 

UlrichRaschke

Re: Kinect for Jack

Experimenter
Experimenter
Hello,

Is the Jack still compatible with Kinect V1 now? Since I just got the new Kinect V2 and adapter, but the Kinect-Jack interface didn't show up when I started it.

Thank you!