Cancel
Showing results for 
Search instead for 
Did you mean: 

Sequential LookAt motion generation

Experimenter
Experimenter

Hi

I am working on JackScript with Jack 8.2 and facing issues in generating sequential head/eye lookat motion using LookAt command.

 

In my scene I have bunch of CAD objects and I want Jack to look at an object for some duration then look at next object. I want to implement this via JackScript. 

 

My current code looks somewhat like this:

Jack.LookAt("eh", scene.object1)

time.sleep(3)

Jack.LookAt("eh", scene.object2)

time.sleep(3)

Jack.LookAt("eh", scene.object3)

time.sleep(3)

Jack.LookAt("eh", scene.object4)

 

However, once I execute script, Jack UI hands for a some time and then directly shows the last LookAt command's result - i.e. in above case it directly shows output of Jack.LookAt("eh", scene.object4). I was to simulate it sequentially i.e. Jack should look at object1 then wait for 3 secs then jump to object 2 and so on. There is no error in python code.

 

Am I wrongly implementing any command? Is there is any seperate command to refresh display window?