Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

TSB Go task creation

Valued Contributor
Valued Contributor

Hello Guys

 

I am a new person for Jack simulation in PS Software.

 

when I created TSB for "Go task", jack can only go in the "Default Posture ", if I changed Jack location or Posture, it can not running Go task, not sure I expalain clearly or not .

 

such as below posture I want jack go ahead

 

Jack1.PNG

but after creat GO TSB, Jack revert back to defalt posture below

 

can I know how to fix it?

 

Thanks

 

Jack2.PNG

4 REPLIES 4

Re: TSB Go task creation

Siemens Legend Siemens Legend
Siemens Legend

Hi,

 

I am not completely sure - but it looks like the environment may be loaded "upside down".

 

TSB will work properly only in an environment where the positive Z direction = up.

 

Is it possible for you to rotate the environment 180 degrees, so it matches Jack's idea of up and down?

Then retest the GO task creation ?

 

Best regards,

Pelle

 

 

 

Re: TSB Go task creation

Valued Contributor
Valued Contributor

so your mean is we only can create the resource and environment in Jack's positive Z direction = up?

 

and all the resource should match with Jack only, if we want to use TSB?

 

not able to change jack to match other resources' Z direction?

 

Thanks

Re: TSB Go task creation

Siemens Legend Siemens Legend
Siemens Legend

Right, if possible please rotate "the world" so it corresponds with pos Z = up.

Some commands will work fine also when Jack is rotated upside down, but TSB in general will not.

 

Best regards,

Pelle

Re: TSB Go task creation

Valued Contributor
Valued Contributor

Thanks, Issue closed base on your direction, but hope in Tecn v13 can be done some improved

 

Thanks