Cancel
Showing results for 
Search instead for 
Did you mean: 

object weight consideration

Experimenter
Experimenter

Hello,

I’m creating a simulation of a box lifting. I wish to analyze it with LBA (low back) evaluation. 

I want the weight of the box to be considered during the entire simulation (and not only for a single posture using the "add load" feature). 

Is it possible?

Yaar

1 REPLY

Re: object weight consideration

Siemens Genius Siemens Genius
Siemens Genius

Yaar,

 

I believe you are using the TSB system in Jack. Weights and forces associated with part manipulation are managed by the TSB system. To apply a weight or force attribute to an object, right click on the part and select TSB->Define Weight or TSB->Define Force from the context menu. These attributes will be applied whenever human figures interact with those objects.

UlrichRaschke