Cancel
Showing results for 
Search instead for 
Did you mean: 

D-Cubed 3D DCM Version 51.0

Siemens Visionary Siemens Visionary
Siemens Visionary

Siemens PLM Software releases Version 51.0 of D-Cubed 3D DCM

 

D-Cubed 3D DCM (Dimensional Constraint Manager) enhancements include:

 

Introduction of a Surface Normal Constraint

3D DCM supports a large range of geometry and constraint types. The latest release introduces a new constraint that makes geometry normal to a surface. The constraint can be applied between a line or a geometry with an axis (such as a cylinder or cone) and a spline, evaluated parametric, spun or swept surface. A typical use of this constraint is to constrain features to freeform faces.

 

Pinning Geometry During Dragging

3D DCM enables users to interact with an under-constrained model by interactively dragging geometry to investigate different configurations while ensuring that the applied dimensions and constraints are satisfied. During dragging it can be helpful to specify that one or more geometries will not move unless necessary. This capability, known as pinning, is introduced in 3D DCM version 51.0. The pinned geometries are free to move again after the dragging has been completed.

 

About D-Cubed 3D DCM

D-Cubed 3D Dimensional Constraint Manager (3D DCM) is a geometric constraint solving software component. Supporting a wide range of geometries, dimensions and constraints, 3D DCM enables 3D parametric sketching, part shape control using direct modeling, assembly part positioning and kinematic motion simulation.