Cancel
Showing results for 
Search instead for 
Did you mean: 

Error in Pretreatment: unable to determine valid rotary positions

Experimenter
Experimenter

I am using an Sim09 (Heidenhain TNC) as start.

I get an error text. See attached file:

 

 

How can I see which of the axis limitation I shall change.

 

Regards

Per

2 REPLIES 2
Highlighted

Re: Error in Pretreatment: unable to determine valid rotary positions

Siemens Legend Siemens Legend
Siemens Legend

Hi Per,

 

difficult to say with only this informations. It depends on the values of operation and the kinematics settings in your post. Is the post created with a machine model or is it created without a kinematic model? What are the limits settings in the post in real machine kinematics properties? Do you change any other settings in the Tilting plane Kinematics or TCPM or use these properties the current kinematics values?

 

Sometimes i prefer the way to first unlimited the 4th and 5th axis to find the reason for it. From your information i would say vectors are correct. But not sure if e.g. the spindle direction is correct?

 

Best regards

Thomas

Re: Error in Pretreatment: unable to determine valid rotary positions

Legend
Legend

Hello 

 

This is a machine which can not work if the tool axis vector component for Z  (mom_tool_axis(2) is less than 0)

So please see in your operation if this happends. 

In other words the plane can only have values from 0 to 90 degree.

 

Hope this helps

 

Error in Pretreatment: unable to determine valid rotary positions

Experimenter
Experimenter

I am using an Sim09 (Heidenhain TNC) as start.

I get an error text. See attached file:

 

 

How can I see which of the axis limitation I shall change.

 

Regards

Per

NX CAM Postprocessor Group
NX CAM Postprocessor Group

Members (207)