Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Help with pretreatment

Experimenter
Experimenter

Hi!

 

I have created an UDE, Now I want to use that variable in the ude at the beginning of the program. How do we use pretreatment so that we can place the udev in the program folder and use it in the programheadern.

 

Regards

Per

 

2 REPLIES

Re: Help with pretreatment

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello working with Post Configurator two functions are important only.

 

1. Make sure the needed data (variable) are stored during pretreatment call.

2. Reuse them later in the post run.

 

Here an overview of the needed functions

Post Configurator_Pretreatment.jpg

Below an example where the fixture offset (e.g. G55) is output earlier in the NC Code.

pretreatment_example.jpg

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: Help with pretreatment

Siemens Phenom Siemens Phenom
Siemens Phenom

One important addition.

If you like to get the data in the header this is the key function to use. I copy that from the docs.

 

program header.jpg

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software
Highlighted

Help with pretreatment

Experimenter
Experimenter

Hi!

 

I have created an UDE, Now I want to use that variable in the ude at the beginning of the program. How do we use pretreatment so that we can place the udev in the program folder and use it in the programheadern.

 

Regards

Per

 

NX CAM Postprocessor Group
NX CAM Postprocessor Group

Members (176)