Cancel
Showing results for 
Search instead for 
Did you mean: 

MOM variable for Wedim thread hole point?

Experimenter
Experimenter

Any idea what is the MOM variable for thread hole point in Control Points for WEDM operation?

4 REPLIES 4

Re: MOM variable for Wedim thread hole point?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There may not be a specific variable for that - it may just be mom_pos and a motion.

I don't know, there may be a mom_evemt_type (or something).

 

What I'd do:

- find the thread about Moog_Show_Globals, download & add to your post in appropriate spot.  I might limit to first 5 motions or something.

- create a wire EDM without start point

- post, and save the info window listing from Moog_Show_Globals to a text file

- add thread hole point

- post, save the info window to a different text file

- compare the text files, see if any differences pop out

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: MOM variable for Wedim thread hole point?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The other option is to turn on the review tool 

- post operation without thread hole

- add thread hole to op & post again

- compare the event listings

- note the review tool creates files you can use (instead of Moog_Show_Globals) so you can compare them.

 

Look for events that get added, maybe there's an event or vaiable you can use.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Highlighted

Re: MOM variable for Wedim thread hole point?

Valued Contributor
Valued Contributor

There is a MOM_thread_wire event. To figure out what should happen and when, you need to to check it with the review tool.

W10 NX12.0.2.9
testing v1847

Re: MOM variable for Wedim thread hole point?

Experimenter
Experimenter

Thanks, looks like getting too complicated with i could imagine.

MOM variable for Wedim thread hole point?

Experimenter
Experimenter

Any idea what is the MOM variable for thread hole point in Control Points for WEDM operation?

NX CAM Postprocessor Group
NX CAM Postprocessor Group

Members (201)