Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Two different values in the same variable

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello,

 

Sometimes the same variable has two or more values in the debugger. Normally it is not a problem because the last value is the correct one.

 

The problem is when the last value is incorrect. What can be done?

 

Example:

 

mom_spindle_rpm= 1570

mom_spindle_rpm=100000

 

Spindle.JPG

 

 

 

 

 

Many thanks in advance,

6 REPLIES 6

Re: Two different values in the same variable

Gears Phenom Gears Phenom
Gears Phenom

hi

I dont know where you get it, in my debug file is always one value in one variable

Probably in your case there is variable set to some default or zero and then event generator set it to correct value later.

so you can see mom_spindle rpm 0 and later 2500 in the same debug file.

But Ive never seen values in one variable in line

sorry f I dont understand

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Two different values in the same variable

Legend
Legend
Sometimes I have this behavior also

Re: Two different values in the same variable

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I reported this (IR7473690) and got some info back. (note mine was for mom_spindle_maximum_rpm, so I guess it is slightly different)

Note we encountered this upgrading from NX7.5 to NX10, so it occurred somewhere in that time frame.

Apparently there is a hard-coded value of 100000 in NX.

If the operation's "max RPM" (in SFM mode) is zero, then 100000 is used instead.

If you set it to a value, or change the op to RPM mode, it went away.

 

I'm wondering if it is a "level" issue in tcl (e.g. "uplevel" command)

The variable/value used over-rides the 100000 value?

 

I guess that's one way to "encourage" users to try out high speed machining ;-)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Two different values in the same variable

Gears Phenom Gears Phenom
Gears Phenom

I have never problem with mom spindle speed. I am using it alwasy in initial/first move. Not sooner.

I have noticed that max rpm , 100000, but I use max rpm if toggle variable is on, or using some workaround, etc..

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Two different values in the same variable

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Thank you both for the replies,

 

Unfortunately I think this it doesn´t solve my issue Smiley Happy.

 

Best regards,

Re: Two different values in the same variable

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

To get the issue solved, you would have to log an incident with GTAC & see what development says.

Be prepared to supply your part & post.

 

To get around the issue now, you might want to check the spindle variables to see if  they are >  90000 (I don't think there's many machines with spindles that fast) and warn the user / abort / whatever.

 

I would check all the settings on the feeds/speeds dialog to see if there was a setting that fixes the issue.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Highlighted

Two different values in the same variable

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello,

 

Sometimes the same variable has two or more values in the debugger. Normally it is not a problem because the last value is the correct one.

 

The problem is when the last value is incorrect. What can be done?

 

Example:

 

mom_spindle_rpm= 1570

mom_spindle_rpm=100000

 

Spindle.JPG

 

 

 

 

 

Many thanks in advance,

NX CAM Postprocessor Group
NX CAM Postprocessor Group

Members (191)