Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

output SMM and RPM (turn PP)

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi,

 

I want to have two different outputs in G code, when I use different Spindle Speed Output Mode.

 

When I use SMM, I need this output:

11.PNG

 

When I use RPM, I need this output:

22.PNG

 

What kind of custom command I need to create.

 

Can someone help me?

2 REPLIES

Re: output SMM and RPM (turn PP)

Gears Phenom Gears Phenom
Gears Phenom

hi

this should work by default / check lathe generic PP.

Only you have to do is edit G codes if necessary. (for example G92 to G50)

 

Output is represented by template blocks. (named spindle_....)

 

*Check also

PB_CMD_spindle_sfm_prestart

PB_CMD_output_spindle

(notice where they are in use)

 

Now you know everything and you can edit it or create your own logic.

 

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: output SMM and RPM (turn PP)

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
ok. I will tested!
Thanks.
Highlighted

output SMM and RPM (turn PP)

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi,

 

I want to have two different outputs in G code, when I use different Spindle Speed Output Mode.

 

When I use SMM, I need this output:

11.PNG

 

When I use RPM, I need this output:

22.PNG

 

What kind of custom command I need to create.

 

Can someone help me?

NX CAM Postprocessor Group
NX CAM Postprocessor Group

Members (161)