Cancel
Showing results for 
Search instead for 
Did you mean: 

NX Continuous Release F.A.Q

Community Manager Community Manager
Community Manager

We've had many questions surrounding NX Continuous Release. We've established a F.A.Q that hopefully answers your questions. Please see below for a list of question and answers.

 

NX Continuous Release | Frequently Asked Questions                                                                                                                                                                                                                        

Siemens will become the first major CAD/CAM/CAE vendor to deliver its software using Continuous Release methodology in January 2019. Below are some frequently asked questions about what customer can expect moving forward with NX Continuous Release and what it means for Simcenter 3D.

 

Q: Why are we introducing Continuous Release?

A: In our regular Voice of the Customer survey our NX customers tell us that they want faster turnaround of product enhancements while maintaining our high quality levels.  The new Continuous Release process will significantly reduce the time between the proposal of a new enhancement, and its deployment to the end users. Customers will now have the opportunity to deploy the latest NX productivity enhancements more quickly in their production environment which helps them become more productive when using NX.  In addition the Continuous Release will also reduce deployment costs for incremental updates.

Adopting a continuous release strategy also allows both Siemens NX and our customers to be more responsive to new ideas and trends in technology, once again allowing our customers to stay ahead of their competition.

 

Q: What problem will Continuous Release address?

A: On average, customers in the PLM industry take at least 3 years to deploy PLM-specific software updates, which means they are not benefitting from hundreds of enhancements and fixes. With Continuous Release customers will have an opportunity to realize our latest advancements in production environment without delay.

 

Q: How will customers benefit from this new Continuous Release strategy?

A: With Continuous Release, customers can now leverage new functionality in their production environment more quickly while reducing the cost of deployment and upgrading. They will also benefit from a tighter feedback loop back to Siemens PLM Software, as well as an increase in responsiveness to new ideas and trends.

 

Q: What gives Siemens PLM confidence that Continuous Release will be successful?

A: Over the last few years, customers increasingly have begun adopting regular monthly Maintenance Pack releases which has reduced the number of customer specific hot-fixes. This demonstrated that our strategy of focusing on protecting customer investment is being recognized and that every NX  and Simcenter 3D release is customer deployment ready. With continuous release, Siemens will continue to improve the upgrade process through quality, product improvements with a focus on protecting customer data.

 

Q: What are the key concepts for Continuous Release strategy?

A: Built on a modern architecture, the NX platform will enable accelerated releases with step-wise enhancements and maintenance that focus on providing new and improved utilities along with process guidance while making it easier for customers to upgrade

 

Q: What are the key changes customers should expect with this new Continuous Release?

A: Customers in Continuous Release mode will see monthly update releases, with major enhancement releases approximately every 6 months.  The monthly updates will be for fixes and a small number of high priority projects. There will be no schema and compatibility related changes in monthly updates.

 

Q: Will the NX support model change in this new Continuous Release mode?

A: Yes, the vision is to have a single release stream. This means that any fix or enhancement will be made only in the latest update released. We are driving in this direction so that we can concentrate all of our development and test effort on the more frequent enhancement and monthly releases, and not to dilute the value of taking the latest update release.

 

Q: Is the traditional NX release numbering changing with the Continuous Release?

A: Yes, with Continuous Release the vision is to remove the focus on release numbering as the ‘decoder ring’ from the mindset of customer in terms of perceived quality and deployment readiness. Each new release is purely “NX”.

 

Q: Who is the target market for Continuous Release and when will it be introduced?

A: All users, ranging from single seat customers through to large enterprises with or without configurations, customizations and integrations will benefit from our new Continuous Release approach which will be introduced in January 2019.

 

Q: Customers have a number of add-on products that are separate downloads, will they be compatible with the new continuous release approach?

A: We will share early builds with our partners to enable them time to ensure compatibility. This early build process will be rolled out in coming months to allow our partners time to be ready for the launch in Jan 2019.

 

Q: Some customers are happy with the current process, why change?

A: Our goal is to make customers as productive as possible with little to no additional cost. This new process as compared to the current process will allow new features and capabilities to be delivered more frequently and more economical.

 

Q: Will Continuous Release affect Beta testing and/or the ability to preview and test early builds?

A: With Continuous Release, we will be looking at ways to make it easier for customers to participate in early Beta testing events and to download and test early builds.

 

Q: Will the new Continuous Process impact existing NX licensing process?

A: Customers with a perpetual licensing model will be able to continue using their existing license request, procurement and install process. 

 

Q: How will NX Continuous Release impact integrations with Teamcenter and Active Workspace from version compatibility perspective?

A: Continuous Release will incorporate new development practices that will remove the need to upgrade currently supported versions of Teamcenter and Active Workspace when updating NX.

 

Q: Will the new Continuous Release process impact the traditional NX or Simcenter 3D download and install process?

A: Customers will still have the option to use their existing GTAC process of downloading updates and enhancements to NX and Simcenter 3D. As soon as an update is released under this new Continuous Release process, it will be available on GTAC for customers to download.

 

Q: Currently I can “roll back” from a point release (from 11.0.2 to 11.0.1 for example) and my data is still compatible, how will this work in the new process?

A: With Continuous Release customers will still have the ability to “roll back” as they do today, however, we will be introducing some validation checks and policies on how far customers can roll back to prevent any compatibility issues.

 

Q: How will Continuous Release impact customer-specific NXOpen customizations?

A: API reports will be published with information on what has changed, as well as tools that can be used to generate a report on how the incoming update will impact customer-specific NXOpen customizations.

 

Q: How will Continuous Release impact customer specific NX configurations?

A: An easy out-of-the-box solution will be delivered as part of the upgrade to preserve all NX configurations automatically during the update. For the most important business-critical NX configuration planning and deployment, reports on what's changed will be published along with tools that can be used to generate a report on the impact the incoming update will have on customer-specific configurations.

 

Q: Will NX documentation be kept up-to-date in this new Continuous Release mode?

A: NX documentation and the What’s New guide will become more valuable with this new Continuous Release model. They will be restructured to enable customers to plan for and accept incoming NX updates.

 

Q: Which applications will be included in the new Continuous Release process??

A: Both NX and NX CAM will be updated through the new Continuous Release methodology. See further in this Q&A on what it means for Simcenter 3D.

 

Q: How do I keep NX up to date?

A: The best way to keep your NX up to date is to turn on automatic updates. With automatic updates, customers do not have to search for updates online and will not miss critical fixes. The NX Update mechanism will automatically notify and installs important updates as they become available.

 

Q: Will it still be possible to run multiple different releases on the same hardware as today?

A: Yes, it will be possible to run multiple versions of NX side-by-side, but only one version will be compatible with the automatic updates. It will be customer’s responsibility to install and maintain NX versions that are not current and automatically updated.

 

Q: How much time is needed to download NX updates to my workstation?

A: The time required to download NX updates primarily depends on connection speed, network settings, and the size of the update. Make sure the workstation is plugged in and connected to the Internet to download and install updates faster.

 

Q: What does the NX Continuous Release strategy mean for Simcenter 3D?

A: Simcenter 3D and NX continue to be fully integrated and fully interoperable with the NX Continuous Release deployment. This means that Simcenter 3D and NX releases and respective release mechanisms will remain fully synchronized and integrated.

 

However Simcenter 3D major releases (which provide major new functional contents) will move to a 6 months release schedule starting January 2019. This means that intermediate NX releases will only include quality releases for Simcenter 3D (= only PR fixes) and exceptionally some minor enhancements.

 

The NX Continuous Release mechanism will thus benefit combined NX – Simcenter 3D customers with faster access to quality improvements for both NX and Simcenter 3D 

 

The NX Continuous Release strategy thus sustains full NX – Simcenter 3D integration and interoperability.

Comments
Solution Partner Valued Contributor

NX has typically allowed reverse compatibility within a major release. Parts designed in NX10.0.3 can be opened in NX10.0.1 but not in NX9.0.X. And of course, I can open this part in NX11.0.x. This lets me jump to the 0.3 release ASAP as a designer and still allows an outside shop to lag behind. How will continuous release handle this? If I adopt continuous release in my orgainization and I've bumped up to the second major release in 2019 (June/July 2019), can the part be opened by the previous version of NX released Jan 2019 (NX version 1847)?

 

Reverse the perspective. As an NX CAM job shop, do I have to maintain continuous release to stay with the latest version of NX in order to support anyting that comes in the door regardles of NX version?

Siemens Phenom

Hi @martinm,

 

The FAQ says:

"With Continuous Release customers will still have the ability to “roll back” as they do today, however, we will be introducing some validation checks and policies on how far customers can roll back to prevent any compatibility issues."

 

As schema changes will only be made in a functional update, which will be available every 6 months, I expect that the data will be compatible to all minor monthly updates delivered in this 6 months timeframe. Updating to a higher functional release may or may not break downstream compatibility to the prior functional release. It is dependent on what is being changed in the system and may even be dependent on what features you used in your parts...

I expect we all need to stay tuned on this one. Still some time to go. But I'm happy communication to the field is done that early so customers have time to prepare. 

 

Johannes 

Experimenter

Siemens, please be realistic and have a look at this article, which is about Microsoft and their Windows 10 strategy about continuous releases:

https://www.computerworld.com/article/3270969/microsoft-windows/what-it-costs-to-keep-up-with-window....

I am afraid the cost to maintain your upgrade tempo will only increase instead of decrease...

Gears Esteemed Contributor

Will there be a notice before/after the update happens?

I might want to save a copy of the install folder to "freeze" that version/release, before the update happens...

Valued Contributor

JCRP, its just natural that when u got updates and if you dont update your hardware in a while you maybe need to upgrade it.

as software envolves hardware also does. Continuous Release is a must have in my opinion, when you want to deliver good product in short time and ez way taking advantage of all comands and technology.

didnt saw any disadvantage on the w10 Continuous release (only if you got a 15year old computer) on the contrary i just see a lot of advantages (if you manage it corretly )
ps. dont want to "hurt feelings" just debate a subject

Experimenter

Romealanuario, thanks for sharing your thoughts about Continuous Releases! I really hope the advantages will be bigger than the disadvantages. If you have a lot of customization running as well as interfacing to other systems (Teamcenter, ERP, sales configurator, ...), then Continuous Releases can be a very delicate affair and one must be very careful with it. While writing this, I think that the openness of NX is a bit in conflict with Continuous Releases. The openness results in the possibility to set up customization and interfacing to other systems. If continuous releases makes a change in the way NX communicates with the outside world (other systems), this has consequences for the customization and interfacing and this can cause extra costs for admins and software engineers. As far as I understand it, the article about windows 10 releases form Gartner I referred to is mainly about that aspect.

Siemens Phenom

@Ken_A:

Yes, the updater includes a notification mechanism for available downloads, download progress, and allows you to control when the update will take place. I do not think you will be able to work with NX while the actual file changes takes place.

And, you do not have to use automatic updates. You can do manual installs as today.

 

@jcrp:

Continuous releases is not in conflict with openness. It does not dictate WHAT technologies or interfaces will be inplemented in NX. But it changes the way WHEN changes can happen. As new technologies emerge faster than ever today (and I guess this trend is ongoing) it is even an enabler to implement new technologies faster than before.

 

But yes, if you update your NX installation every 30 months (2 traditional NX release cycles), you need to verify our NX Open customizations only once in 30 months, too. With continuous releases, API changes can happen more often. Therefore, a tool will be provided to analyze your customizations and find if there is any deprecated functionality used. And there will also be a policy in place about support of NX Open legacy calls/classes, so you may not even need to analyze your customizations with every functional release.

A bit more information has been provided along with the beta test.

 

By the way, Siemens is first supplier of complete design-to-manufacture software to certify with the international Code of PLM Openness. Read this press release and see this article if you are interested.

 

Hope that helps.

Creator

Guys, maybe I overread it, but what happens if you are still on NX9? Does this change also from NX9 on automatically or do we need a special license to get this continuous release? Thank you!

Siemens Phenom

Hello @FranzS,

 

For NX 9.0 nothing will change. You will simply just have to upgrade to NX  "Continues Release", in the same way as you would have as with upgrading to i.e. NX 12.0.

You just need your latest license file, with the correct version in it (if you have active maintenance, you should receive this, when the next version of NX is released), from there onward you can use the automatic update option.

So at least for this one time, you will still need to upgrade yourself. it will not be pushed automatically.

 

Kind regards,


Dennis

Experimenter

How would this work in a regulated industry where software tools must be validated?

Gears Esteemed Contributor

Just disable automatic updates and update manually as you have done before.