Cancel
Showing results for 
Search instead for 
Did you mean: 

NX on Amazon Appstream 2.0 Deployment Guide

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Late last year, Amazon Web Services (AWS) launched new graphics instances on AppStream 2.0.  To try out these instances, the NX Product Marketing team configured NX CAD on AppStream 2.0 and recorded a video to show the fluid and responsive experience of streaming NX CAD. You can read about it and watch the video here.

 

NX_AS2_p3.png

Since then it has generated a lot of enthusiasm in the user community and several NX CAD users have experimented with this setup. It has also been covered in dedicated sessions at user conferences such as PLM Connections, PLM Europe and Regional User Group meetings. Customers who have tried it had a very positive experience. Jonathan Gibney, Vice President of Engineering at Myotek had this to say:

 

“Myotek is a leading Tier 1 automotive supplier based in Irvine, CA. The highly-dedicated team of Design & Manufacturing engineers at Myotek use Siemens NX to develop its well-known innovative lighting solutions for the automotive industry.

 

In order to stay competitive in the automotive industry, lowering the IT infrastructure cost while enabling our team of engineers and contractors easy and secure access to our design software and CAD data is a top priority. Running NX CAD on AppStream 2.0 helps us provide the scalability & flexibility that come with running applications in the cloud. With this solution, we are benefiting from the latest advances in computing without the need to upgrade and maintain desktop workstations.

 

Siemens NX on AppStream 2.0 performs as if you were running the software locally on your machine. However, we get the added benefits of lower costs, increased accessibility and improved collaboration within our team. We know that our data is secure as it stays in a centrally managed environment and don’t have to worry about managing installations and security on each user’s computer.”   

 

AS2_02_768x384.png

 

The benefits of running NX on AppStream 2.0 are numerous:

  • Reducing infrastructure costs by replacing high-end workstations with mobile workstations and paying only for what you use
  • Centrally manage NX installations and simplify roll out of software updates
  • Enhance collaboration by allowing access to more users and thus accelerating product development workflows
  • Give users a fluid and responsive experience with cloud installation of NX designed for their use cases
  • Strengthen security by keeping your data on AWS- only encrypted pixels are streamed to end users through a secure streaming gateway over HTTPS, making them firewall friendly.

 

 

NX on AS2 guide image.pngAfter additional testing of NX on AppStream 2.0, we collaborated with the AWS team to develop a detailed step-by-step deployment guide for this setup so that users have the flexibility to install and run their existing licenses of NX from a cloud environment. The guide is attached to this post and is also available on the Amazon AppStream 2.0 resources page.

 

So if you are interested in trying it out, please download the guide and let us know your feedback.

Comments
Solution Partner Legend

Very useful info, thank you. 

 

Can you explain why the guide recommends to disable the Google Chrome Update Service and why this does not impact application or data safety?

Siemens Valued Contributor

Hello  @Sebastian5050,

 

Happy to know you found the guide useful.

 

The recommendation to turn off the update service is based on the guidance from AWS. As per AWS, many applications have embedded http help links within the application. If you don’t turn off IE ESC, then Windows will prompt an error dialog every time when you click on a link.

Genius

The advantage of streaming an app is obvious, but when will we be able to do this with a managed session of NX?  Of all the various virtualized and/or streamed solutions I've always seen only native NX or Teamcenter w/o CAD integrations.  Never the two together.  There's obvious complexity in streaming or otherwise abstracting the entire stack but there has to be some plans to mitigate for the future.

 

Also a question regarding Appstream and AWS Gov Cloud for using streamed NX with important IP up to and including ITAR data.  According to the docs, GovCloud doesn't support Auto Scaling for AppStream 2.0 fleets.  I'm assuming that means you can still use AppStream 2.0 fleets with GovCloud, you just have to manage your user load manually.  Is that a correct understanding? 

Siemens Theorist

NX Managed Services now supports managed NX Appstream connected to Cloud based Teamcenter.  I do not know what industry vertical you are interested in, but customers can initially engage with Rahul Sharma. 

Also, from your input, we are looking into producing a second guide with help for various streaming setup sceanrios of NX together with TC.

Dreamer

Thank you so much truly a cognitive concept. I do appreciate the effort and hope to get more information.