Cancel
Showing results for 
Search instead for 
Did you mean: 

NX Design Blog

You can use NX expressions to control the relationships between the features of a part, or between parts in an ...
The NISSAN ZEOD RC is the first hybrid vehicle to drive 300 km/h and complete a full lap of the circuit on pure electric power at the 24 hours of Le M...
The NX Assembly Sequence commands can be used to simulate assembly and disassembly of components...
Using NX™ software, Foton eliminated information isolation between departments, and incorporated engineers’ design experience into the system, saving....
The Assembly Sequence commands are used to simulate the assembly and ...
In our new NX Quick Tip, John Baker shows how to create an assembly sequence extraction path for...
NX 9.0.2 is now available for download...
Complimentary 40 page eBook, "Engineering Manager's Survival Guide" just for completing a survey from Lifecycle Insights...
Manufacturer increases productivity by about 20 percent with the help of NX...
Developing injection molds gets easier – and faster – with the help of...