Cancel
Showing results for 
Search instead for 
Did you mean: 

İnferred Dimension command Decimal places setting in drafting

Valued Contributor
Valued Contributor

Hello friends ,

How can we change decimal places in drafting inferred dimension command ? 

i tired change with costumer defaults.

it has setting about decimal places but it works after put dimension.

i need change in command. 

 

2015_06_10_15_53_59_NX_8.5_Drafting_model4.prt_Modified_.png

 

 

Kind Regards,

Alican

 

4 REPLIES

Re: İnferred Dimension command Decimal places setting in drafting

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Changing the customer defaults will only affect new, BLANK files; changes to the customer defaults will have no effect on existing files.

 

To make that change in an existing file, open the file and go to Preferences -> annotation (or preferenes -> drafting depending on your version of NX) and make the desired change there.

 

If you want new files to have this change you must make this change in the template file (or in the customer defaults in you create BLANK files).

Re: İnferred Dimension command Decimal places setting in drafting

Siemens Phenom Siemens Phenom
Siemens Phenom

These settings are part of a Drafting Standard which once you've made those changes in Customer Defaults and you've saved the Drafting Standard settings and restarted NX, after opening a Drawing file, go to...

 

Tools -> Drafting Standard...

 

...and select your new saved standard.  Now you existing Drawing will be using the settings for this new Drafting Standard.  Note this still will not change any existing dimensions, those will have to be edited, but it should affect any new dimensions created.

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: İnferred Dimension command Decimal places setting in drafting

Valued Contributor
Valued Contributor

Thank you . 

Re: İnferred Dimension command Decimal places setting in drafting

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Note there are 2 kinds of settings in customer defaults:

- session settings (these will be used when a session starts, subject to dialog memory)

- part settings (these will ONLY be used if you create a part "from scratch" (using a "blank" template).  Otherwise the part settings will over-ride the customer default settings, unless you do something like John suggested.

 

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled