Cancel
Showing results for 
Search instead for 
Did you mean: 

2-ways tapered cylindrical part

Builder
Builder

Hi,

 

Maybe not the correct forum to ask, but I'm having difficulty realising a cylindrical model that's tapered 2-ways.

As shown here:

 

2017-06-27 10_56_35-NX 11 - Modeling - [model1.prt (Modified) ].png

 

 

How do I do this?

 

 

9 REPLIES 9

Re: 2-ways tapered cylindrical part

Siemens Phenom Siemens Phenom
Siemens Phenom

Could you possible create a sketch in isometric or show what you want in side, front and/or top views? Having difficulty understand what you want to do.

Steve V

Re: 2-ways tapered cylindrical part

Builder
Builder

Hello,

 

Maybe this displays better what I'm trying to do:

2017-06-27 15_40_44-NX 11 - Modeling - [model1.prt (Modified) ].png

The flat part stays untouched.. the rest of the "block" tapers on the inner dia. to minus 0.5mm and the outer dia. to minus 1mm. But I'll have to taper it 2-ways, but I'm not sure how to.


Re: 2-ways tapered cylindrical part

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There's probably a dozen ways to accomplish that, one way is to create a through curve sheet body with the desired start/stop locations for the taper. Attached is a quick & dirty NX 9 model as an example.

Re: 2-ways tapered cylindrical part

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

Here is what i achieved (not sure if this is what you seek)

Taper.jpg

 

I used a helical sweep for the cut (but i could not achieve the straight line transition edge between the FLAT and the tapered area)

Best Regards

Kapil

Re: 2-ways tapered cylindrical part

Phenom
Phenom

Try this.

Double click features and edit this dynamic model to your desired values and model will update accordingly.

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: 2-ways tapered cylindrical part

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Hi @MKarsten,

 

Does the resultant surface need to be planar?

 

Regards, Ben

Re: 2-ways tapered cylindrical part

Builder
Builder

To all: Thank you very much!

 

@mike_fdo your model is exactly what I needed.

Re: 2-ways tapered cylindrical part

Siemens Phenom Siemens Phenom
Siemens Phenom

I think making it planar will be quite difficult (rather impossible)...as the plane only needs 3 points for definition and the one given in the image need 4 points so i guess it might be a warped (sorry 4 point patch) surface.

4.jpg

Re: 2-ways tapered cylindrical part

Siemens Phenom Siemens Phenom
Siemens Phenom

so sorry i think i am too late for this suggestion but in case you want to try it.

 

1_1.jpg

1_2.jpg

 

Best Regards

Kapil