Cancel
Showing results for 
Search instead for 
Did you mean: 

2D Drafting - Trim Dimension Line

Experimenter
Experimenter

Hello, want to change the length of that dimension line. How can I do this? Searching for any value by using Annotation Preferences and Tab Line/Arrow without success.

 

Trim Dimension Line.jpg

2 REPLIES 2

Re: 2D Drafting - Trim Dimension Line

Siemens Phenom Siemens Phenom
Siemens Phenom

Try to change the length of the arrow head so that direction of arrows will be inside out. I am not sure if the length of arrow lines can be controlled through settings/preferences.

Re: 2D Drafting - Trim Dimension Line

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

That is controlled by the "dimension arrow out length factor" which you can find in the drafting standard of your customer defaults. I believe that it is defined as a multiple of the dimension text height and the length cannot be directly controlled. On existing dimensions, this value cannot be edited directly.