Cancel
Showing results for 
Search instead for 
Did you mean: 

2D Shell analysis question

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hello,

I'm new to NX. Trying to solve simple model with 2D mesh.
One edge is fixed, another is loaded with vertical force. Material is usual Steel from NX library.
Below I post the displacement result plots. Looks like only side plates are working properly. 
What am I doing wrong? Thanks

question1.pngquestion2.pngquestion3.png

2 REPLIES

Re: 2D Shell analysis question

Valued Contributor
Valued Contributor

If I see it correctly the meshes are not connected at the edges of the sheets. You can use stitch to connect them.

 

- Jelle

Re: 2D Shell analysis question

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Everything seems to be stitched, there are no duplicate nodes. 
Anyway I tried to stich once again and recalculate. Nothing changed.