Cancel
Showing results for 
Search instead for 
Did you mean: 

AUTO MAP DRIVE ISSUE PLUS SLOW LOADING OF ASSEMBLIES IN NX10

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello all,

 

One of my user is facing an issue they have connected to auto map drive but when ever they open nx auto map drive folder is creating as an shortcut and after closing it'll close and it is taking a lot of time while opening assembly files

 

 

 

any suggestions????

2 REPLIES 2

Re: AUTO MAP DRIVE ISSUE PLUS SLOW LOADING OF ASSEMBLIES IN NX10

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Ho do you go to the drive? By a script or with windows mapped drives?

 

 i had a same issue with a script mapped drive, after i mapped the drive manually to the user and configured windows startup to allways stay connected to the drive it worked

Re: AUTO MAP DRIVE ISSUE PLUS SLOW LOADING OF ASSEMBLIES IN NX10

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Thanks mate ..issue resolved