Cancel
Showing results for 
Search instead for 
Did you mean: 

Add Material in Part Families

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

Hi there,

 

Anybody knows how to add material in Part Families?

 

I attached to model a material by using Asign Material command, but when I choiced Material collumn in the Part Families command, the alert shows like image below:

 image.png

 

Bauler

NX 12 | TC 11.4 | Win10

2 REPLIES 2

Re: Add Material in Part Families

Phenom
Phenom

Hi @bauler,

maybe the message it's not so clear. Please refer to the help page.

Thank you...

Using NX1859
RuleDesigner PDM

Re: Add Material in Part Families

Siemens Phenom Siemens Phenom
Siemens Phenom

bauler --

 

As the message states, naming the solid body is the key here.  You can assign a name by right-clicking on the solid body (specifically the solid body, and not a feature) and adding it here in the "General" tab:

 

2018-08-25_12-31-02.png

 

Once you've done that, the body will be available for inclusion in the part family spreadsheet when you choose Material from the Available Columns option menu:

 

2018-08-25_12-30-03.png

 

...and if you set up your spreadsheet something like this:

 

 

2018-08-25_12-25-51.png

 

Then the part family children will take on the appropriate new density based on the identified material:

 

2018-08-25_12-24-43.png

 

Hope that helps!

Taylor Anderson
NX Product Manager, Knowledge Reuse and NX Design
Tel: +1 (602) 441-0683
taylor.anderson@siemens.com