Cancel
Showing results for 
Search instead for 
Did you mean: 

Add same part to assembly mirrored ?

Genius
Genius

Hi

How to add a same part but mirrored in assembly ?

- I now press Add Part and use Move+Constraints to place the part.

Mirrored part add assembly.jpg

I tried this ?

  • What is the difference between these 4 pcs ?

mirror assembly.jpg

 

4 REPLIES

Re: Add same part to assembly mirrored ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Re: Add same part to assembly mirrored ?

Valued Contributor
Valued Contributor

But the "Mirror assembly" does not add the constrains,just the part. So you have to constrain the part anyway. In this case I would use "move with copy"  and than fix it on the place. Seems as quicker way  to me .

Re: Add same part to assembly mirrored ?

Siemens Phenom Siemens Phenom
Siemens Phenom

If mirror assembly command is not working for the condition you are trying, You can mirror body inside part, create the reference sets and use while adding it in assembly.

Regards,
Ganesh Kadole
#IngenuityIsNX | NX - What's New

Re: Add same part to assembly mirrored ?

Legend
Legend

Is it the same part or a mirrored (symetrically opposite ) part?

Sometimes they are the same thing, other times not.

 

If its the same part number, I'd reposition and constrain it. If its a sym-opp part. makes a kinked mirrored body then position and constrain it.

 

 

Rob Newcomb, CAD/CNC/Simulation manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.2 / Autoform r7 /WorkNC 2018 r2
Testing:NX EAP
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro