Cancel
Showing results for 
Search instead for 
Did you mean: 

Adding items to the pop-up menu.

Creator
Creator

How does one add items to the pop-up menu.  This was possible in past versions.

The option does not seem to be available.

5 REPLIES 5

Re: Adding items to the pop-up menu.

Siemens Phenom Siemens Phenom
Siemens Phenom

Customize (Ctrl+1)

Under 'Shortcuts' tab you can find the three different application radial options that you can customize.

 

Radial Pop up.png

 

Re: Adding items to the pop-up menu.

Creator
Creator

Thanks again. The option is still there and I missed it.

Re: Adding items to the pop-up menu.

Gears Phenom Gears Phenom
Gears Phenom
Note that those are Radial Popup menus - there is another (MB2 in graphics window) called View Popup. It helps us know to which you're referring when you're asking that particular question.
Tim
NX 11.0.2.7 MP11 Rev. A
GM TcE v11.2.3.1
GM GPDL v11-A.3.5.1

Re: Adding items to the pop-up menu.

Creator
Creator

Yes, and my original question pertained to the MB2 View Popup. My question did not specify (my fault).

However, I got my answer and appreciate your help!

Re: Adding items to the pop-up menu.

Gears Phenom Gears Phenom
Gears Phenom
Yes, same general area of customization - just makes it clearer to those wishing to help.

You can also go into that same menu tab, select a particular object (if you have a model or drawing open) and customize the popups that appear when you preselect those same objects. This can result in reducing a TON of mouse travel.
Tim
NX 11.0.2.7 MP11 Rev. A
GM TcE v11.2.3.1
GM GPDL v11-A.3.5.1