Cancel
Showing results for 
Search instead for 
Did you mean: 

Adding part with note part to assembly

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi everyone,

 

I want to add part with some notes on one face to assemby, but when I try to do that I loose all notes on this face. Someone has similiar problem? What could be reason? In attachment I sensd some screenshots to better understand probleM.

 

BEST REGARDS

LUKIPAPERROR_BELMA.png

4 REPLIES 4

Re: Adding part with note part to assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Guessing, one or both of:

- Notes are not part of the reference set used in the assembly (try using "Entire part" reference set)

- Notes are on a layer that is turned off in the assembly

 

It might be other things, but that's what I would check first

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Highlighted

Re: Adding part with note part to assembly

Gears Phenom Gears Phenom
Gears Phenom

Or notes have been created view-dependant... Not sure what happens to these in an assembly context.

Graham Inchley Snr R&D Engineer (Systems Development), Sandvik Coromant
Dell 7530 Precision, Win10, 32GB. Developing in: Java | C | KF
Production: [NX12.0.2 MP1]

Re: Adding part with note part to assembly

Siemens Phenom Siemens Phenom
Siemens Phenom

How did you create these notes? Did you use the PMI application to create them? Or are they created some other way (using the Notes Drafting command, for example?).

Re: Adding part with note part to assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Or modeling text?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled