Cancel
Showing results for 
Search instead for 
Did you mean: 

Adjust value instead of zoom in/out

Phenom
Phenom

Is there a way to set NX so that when a input field is active that you can increase/decrease the value using the scoll/roll mouse button- Middle mouse button?

2 REPLIES

Re: Adjust value instead of zoom in/out

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Hi @RyanM,

 

We have a similar, existing Enhancement Request: ER 5210013 "Use the scroll wheel to edit dimensions dynamically".

 

Regards, Ben

Re: Adjust value instead of zoom in/out

Siemens Phenom Siemens Phenom
Siemens Phenom

@RyanM,

If you have sketches, you can do this while a sketch is active using the 'Edit Parameters' option. Also, if you create PTS templates for your reusable components, then in the UI you can define your inputs to be slider bars which would enable you to do the same as in a sketch. Other than that, file an ER as Ben suggested.

(view in My Videos)

Regards,
Abe