Cancel
Showing results for 
Search instead for 
Did you mean: 

Adjustable properties of layers

Creator
Creator

Why i can't adjust the properties of parts using layer?
It so strange that NX doesn't have opportunity to adjust width of line, color, type of line by layer.
Is it so hard to make this oprion in 3D modelling and drafting?

2 REPLIES 2

Re: Adjustable properties of layers

Gears Phenom Gears Phenom
Gears Phenom
@Alex1985,

Were you aware that you can select objects on specific layers (as well as a plethora of other selection filters) then use Edit Object Display and change line width, colors, line fonts? NX has some pretty powerful pre-selection / selection filtering tools available.
Tim
NX 11.0.2.7 MP11 Rev. A
GM TcE v11.2.3.1
GM GPDL v11-A.3.5.1

Re: Adjustable properties of layers

Creator
Creator

 

Why? why i have to do so much movements????

Do you see difference betwen layer menu adjusting or select each object on each layer and udjust it? Of course you understand that i have to hide other layers before and show it after.

Or you think i have so much time for all this stuff?