Cancel
Showing results for 
Search instead for 
Did you mean: 

After TC11 and NX11 update tangent lines are visible ?

Genius
Genius

Hello

After TC11 and NX11 update tangent lines are visible ?

Sheet metal -> Flat-Pattern -> Drafting

- I have imported my NX9 customer defaults in to NX11.

- But I still get visible green tangent lines to my Flat-Patterns (Which were invisible when using NX9).

- How to remove tangent lines from flat-patterns ?

 

flatpatterncustomer.jpg

4 REPLIES 4

Re: After TC11 and NX11 update tangent lines are visible ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @12131444,

Go to the flat pattern view settings, under inherit select the settings source to customer defaults > Click on the icon next to 'Load from Settings Source' and click on Apply button.

 

sheetmetal.png

Re: After TC11 and NX11 update tangent lines are visible ?

Siemens Phenom Siemens Phenom
Siemens Phenom

You can also inherit the customer defaults settings in same way for the drafting preferences.

Menu > Preferences > Drafting > Inherit settings.

Re: After TC11 and NX11 update tangent lines are visible ?

Genius
Genius

When I click Apply it goes back to "Preferences"-source and "Customer default"-source disappears.

 

Why "Customer default"-source does not stay ON ?

backto.jpg

Re: After TC11 and NX11 update tangent lines are visible ?

Genius
Genius
Those green lines were "Inner mold line" and "Outer mold line". Now they are invisible.