Cancel
Showing results for 
Search instead for 
Did you mean: 

After start NX (1847) has stopped working

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Error.png

 

Server is running.

 

Thank you

 

Mike

4 REPLIES 4

Re: After start NX (1847) has stopped working

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Did you try re-installing NX?

Re: After start NX (1847) has stopped working

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @MIXA !

 

A "...stopped working" message like that is coming from Windows, not NX, and is typically some conflict at the OS level such as Drivers, etc... I've seen numerous postings on this when running NX, and solution seems nearly always a driver issue.

 

Do you have a Space Mouse?

 

GTAC has posted several docs on an issue there that can lead to this message, most recently 2 weeks back with FAQ-002-7004597, walking you through how to test and update to the latest driver:

 

https://solutions.industrysoftware.automation.siemens.com/view.php?si=002-7004597

Re: After start NX (1847) has stopped working

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

 

Sebastian5050

I did it twice.

Re: After start NX (1847) has stopped working

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

@PatMcManus wrote:

Hi @MIXA !

 

A "...stopped working" message like that is coming from Windows, not NX, and is typically some conflict at the OS level such as Drivers, etc... I've seen numerous postings on this when running NX, and solution seems nearly always a driver issue.

 

Do you have a Space Mouse?

 

GTAC has posted several docs on an issue there that can lead to this message, most recently 2 weeks back with FAQ-002-7004597, walking you through how to test and update to the latest driver:

 

https://solutions.industrysoftware.automation.siemens.com/view.php?si=002-7004597


 

 

Dear PatMcManus

Thanks for advise.

I dont use SM.

I think you are rigth it is driver issue.

 

Best regards MIXA