Cancel
Showing results for 
Search instead for 
Did you mean: 

Aligning hex rivet nuts to hex holes ?

Valued Contributor
Valued Contributor

Hi

How to make hex rivet nuts aligning to hex holes faster ?

  • Now I use Move ->Touch align to every faces randomly to align it. Sometimes it works but through numerous alignings...
  • (Note: no constrains used in this company so Move is used)

Align hex nut.jpg

2 REPLIES

Re: Aligning hex rivet nuts to hex holes ?

Siemens Phenom Siemens Phenom
Siemens Phenom

If the hex holes were created using patterns, then you can use Pattern Component with the Reference option.

This will fill all of the holes with rivets after placing the first one.

 

Another solution is to use Assembly Constraints.  Refer to 'Remember Constraints' in the Help Documentation.

 

Having a 'no constraints' policy in place is something that you may want to re-evaluate.

Re: Aligning hex rivet nuts to hex holes ?

Phenom
Phenom

Use Move Component>Transform> Constraints>Centre ; Subtype> 2 to 2;

 

Then select two opposite faces of the moving part and then corosponding two faces of the hex hole.

 

mf_move_20170125.JPG

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW