Cancel
Showing results for 
Search instead for 
Did you mean: 

Any way to lock toolbars?

Creator
Creator

Is there any way to currently lock toolbars? I love the customization available in the ribbon, but I am constantly re-ordering my tabs because they can be so easily dragged and dropped. Would be nice to have them locked unless I'm customizing my layout... 

 

I hope I'm just missing this... 

 

Kevin

3 REPLIES

Re: Any way to lock toolbars?

Gears Phenom Gears Phenom
Gears Phenom

If you re-apply your role, I think they will go back to your "default" location.  Just have to remember to keep your role updated. 

-Dave
NX 11 | Teamcenter 11 | Windows 8.1

Re: Any way to lock toolbars?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There's save / load roles

 

There's also the Preferences -> user interface -> Layout -> Save layout at exit (un-check so you don't save).  But then if you want to make a change, you have to make the change, then remember to turn it back on, exit NX (so the user.mtx is updated), start NX, turn off the preference again.

 

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Any way to lock toolbars?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

But I agree it would be nice to have a preference to "lock the ribbon layout" to prevent accidental discombobulation...

 

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled