Cancel
Showing results for 
Search instead for 
Did you mean: 

Appended text not working?

Honored Contributor
Honored Contributor

NX 9.0.3.4 mp3

 

This happens with dimensions on a drawing, and pmi dimensions.  More often than not, when you want to add appended text, while placing the dimension, nothing will enter into the quick pop-up appended test input area.  You have to go to the "edit appended text" window.

 

We have had this happen with at least 2 users, including myself.  I've had it work, go to the next dimension, and not work.  Once it quits, it's done.  I've been able to capture it not working on video, and submitted an IR to GTAC, but they can't reproduce it.

 

Curious if anyone else has run into this, and if so, have you found a pattern to way to trigger it?

 

-Dave

-Dave
NX1867(if it had versions) | Teamcenter 11.6 | Windows 10