Cancel
Showing results for 
Search instead for 
Did you mean: 

Area Fill to color Flat-Patterns ?

Genius
Genius

Hello

I used Area Fill to color Flat-Patterns:

  • Now all measures under Area-Fill are invisible when PDF is created ?
  • Why PDF hides measures under Area-Fill ?

 

dadaad4242.jpg

8 REPLIES

Re: Area Fill to color Flat-Patterns ?

Siemens Phenom Siemens Phenom
Siemens Phenom

In your previous post you asked how to use color fill for flat pattern How-to-color-a-flat-pattern.  It would helpful to understand why you do this (see my question in linked post).  Maybe 'fill' is not the correct method for your purpose?

thanks

Re: Area Fill to color Flat-Patterns ?

Genius
Genius
To make a Flat-Pattern sheet metal more visible also enlarging the outlines of the Flat-Pattern would help.
Now lines coming from bend annotations and dimensions are difficult to separate from the Flat-Pattern outlines.

Re: Area Fill to color Flat-Patterns ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

Sorry i do not have NX9 (which i suppose you are working right now) but in NX11 it seems possible . Below is the setting i used for making annotations visible in an AREA FILL.

pdf_chk1.jpg

 

Here is the PDF exported out of it.

pdf_check2.jpg

 

Best Regards

Kapil

 

Re: Area Fill to color Flat-Patterns ?

Siemens Phenom Siemens Phenom
Siemens Phenom

It is also available in NX 9.

 

sm ant.PNG

 

Regards,
Ganesh
#IngenuityIsNX | NX - What's New

Re: Area Fill to color Flat-Patterns ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Thanks for validating Ganesh.

Regards

Kapil

Re: Area Fill to color Flat-Patterns ?

Siemens Phenom Siemens Phenom
Siemens Phenom

@12131444 wrote:
To make a Flat-Pattern sheet metal more visible also enlarging the outlines of the Flat-Pattern would help.
Now lines coming from bend annotations and dimensions are difficult to separate from the Flat-Pattern outlines.

I would recommend setting up your sheet metal and drafting template preferences to define the line widths for flat pattern views.  Once set, the outlines should be clear and you then have no need for the extra step of color fill.

Sheet Metal Preferences-->Flat Pattern Display

Drafting Preferences-->View-->Flat Pattern

2017-04-18 08_21_25-NX 11.0.1.11 - Drafting - [sheet_metal_model4.prt (Modified) ].jpg

I hope this helps.

Re: Area Fill to color Flat-Patterns ?

Genius
Genius

What are the default selections or values for outline, contour thickness ?

 

52525.jpg

Re: Area Fill to color Flat-Patterns ?

Siemens Phenom Siemens Phenom
Siemens Phenom

NX out-of-the-box, the defaults are 'Solid' Font and 'Normal' line width (Customer Defaults-->Sheet Metal-->Flat Pattern-->Curves)

The actual values for line widths are defined in Customer Defaults-->Line Widths.

 

If you created a Template for new files, these values will be stored there.

 

Setting up templates and defaults for each file type is totally configurable.

2017-04-18 09_34_22-New.jpg