Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Artifacts stay on some parts when repainting ?

Genius
Genius

Hello

In assembly only: ( When "Make displayed part" it is ok )

Why artifacts stay on some parts after re-coloring ?

Color ID: 129=medium Steel is partially visible.

Specific Component color is OFF.

 

Untitled12.jpg

4 REPLIES 4

Re: Artifacts stay on some parts when repainting ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

Did you check the Reference set of the component? Perhaps there are multiple bodies (some sheets etc.) which are included in the Model reference set. You can check the part (for any extraced sheet etc.)

Best Regards

Kapil

Re: Artifacts stay on some parts when repainting ?

Genius
Genius

From I-deas body:

 

assasf2.jpg

addadd.png

Re: Artifacts stay on some parts when repainting ?

Genius
Genius
I gave up and did the "Cleanup body".

Re: Artifacts stay on some parts when repainting ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

When you use Sheet Metal From Solid then it takes reference of the original body and does not consume it alltogether.

 

Make the part a Displayed Part and then go to Format-Reference Sets and deselect the original body in the Model Reference Set.

 

ref_set.jpg

 

Best Regards

Kapil