Cancel
Showing results for 
Search instead for 
Did you mean: 

Assembly Constraints - CSYS to CSYS

Creator
Creator

Is there any way to assemble CSYS of child part to Parent part CSYS in one click?

2 REPLIES 2
Highlighted

Re: Assembly Constraints - CSYS to CSYS

Siemens Phenom Siemens Phenom
Siemens Phenom

It will take at least TWO clicks since there could be multiple CSYS's in both the new Component and the Assembly so you will have to indicate/select the desired CSYS in BOTH the new Component as well as the Assembly.  If that's acceptable (and there is no other choice) then yes, just use the 'Touch Align' Type constraint and select, as indicated above, the desired CSYS's.

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: Assembly Constraints - CSYS to CSYS

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

There is a way to assemble parts in one click. If the component you are adding has a saved assembly constraint, then it will actually be one click - you will only need to pick up one CSYS.

 

Assembly > Component Position > Remember Assembly Constraints.